IMX8 imx-image-full qt5 pkg connection issue with VPN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 imx-image-full qt5 pkg connection issue with VPN

ソリューションへジャンプ
1,894件の閲覧回数
lchen
Contributor III

Hi,

I have successfully build imx-image-multimedia image for imx8qmmek. When I built imx-image-full image or SDK, the qt related pkgs always stuck at do_fetch job if my building machine is connected to company VPN. If I disconnect VPN and just use home network, the qt pkgs fetching works fine.

Is it because company firewall is blocking qt5 source? I can access the qt5 github from the browser.

Thanks,

Lijun

0 件の賞賛
返信
1 解決策
1,880件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
1,889件の閲覧回数
lchen
Contributor III

Never mind, I retried and passed this time.

0 件の賞賛
返信
1,881件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

(y)

 

0 件の賞賛
返信