IMX8 and M4 Memory access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 and M4 Memory access

1,633 Views
mohamed_elsemel
Contributor I

Hello 

I am using IMX8 and i need (for some testing) that both cores A35 and M4 have access to the whole RAM 

how this could be done ?

Thanks in advance 

0 Kudos
Reply
1 Reply

1,595 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mohamed

first may be useful to check: https://community.nxp.com/docs/DOC-341481 

Example of shared memory can be found in function sc_err_t board_system_config()
../platform/board/mx8qm_mek/board.c   SCFW Porting Kit

Also additional details were sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply