IMX8 and M4 Memory access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 and M4 Memory access

1,996件の閲覧回数
mohamed_elsemel
Contributor I

Hello 

I am using IMX8 and i need (for some testing) that both cores A35 and M4 have access to the whole RAM 

how this could be done ?

Thanks in advance 

0 件の賞賛
返信
1 返信

1,958件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mohamed

first may be useful to check: https://community.nxp.com/docs/DOC-341481 

Example of shared memory can be found in function sc_err_t board_system_config()
../platform/board/mx8qm_mek/board.c   SCFW Porting Kit

Also additional details were sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信