IMX8 Quadmax MEK Android Automotive 11 touch input support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 Quadmax MEK Android Automotive 11 touch input support

Jump to solution
3,647 Views
tranvanmau
Contributor II

Hello,

We plan to use 8QuadMax MEK and MX8-DSI-OLED1 touch screen for our R&D project. Android_automotive-11.0.0_1.1.0 is OS.
However, [android_automotive-11.0.0_1.1.0_docs, Android_Release_Notes.pdf, Table 2. Features] only says that for "UI (input)" USB mouse is supported.

What about touch input? Can we use touch screen of MX8-DSI-OLED1 as UI input on 8QuadMax MEK Android_automotive-11.0.0_1.1.0 release?

Could someone help us to answer this question?

0 Kudos
Reply
1 Solution
3,622 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tranvanmau,

The touch screen works on MX8-DSI-OLED but for Android automotive you must check with professional services:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Regards

 

View solution in original post

0 Kudos
Reply
5 Replies
3,613 Views
tranvanmau
Contributor II

Hello Bio_TICFSL,

Thank you for your info, I understand it.

Best regards,

0 Kudos
Reply
3,590 Views
dzvernik_gk
Contributor I

Hello @tranvanmau ,

Did you figure out if the it's possible to use this touch screen (MX8-DSI-OLED1) with the Android Automotive 11 [android_automotive-11.0.0_1.1.0] and it's support out-of-the-box ? 

 

@Bio_TICFSL could you please advice on availability of the MX8-DSI-OLED1 with any distributor since we figured out that there is no availability, at lest not online ?

 

Thanks.

Kind Regards.

0 Kudos
Reply
3,555 Views
tranvanmau
Contributor II

Hello @dzvernik_gk,

I did not know it yet. I closed this thread because the question needs special support from NXP.

Anyway, MX8-DSI-OLED1 is considered to be small (5.48 inch) for our project, so we are thinking of other approaches.

May be some USB touch screens out there can be used (such as this one https://www.viewsonicglobal.com/public/products_download/user_guide/Display/TD1655/TD1655_UG_ENG.pdf...)

Best regards,

0 Kudos
Reply
3,255 Views
tranvanmau
Contributor II

We buy this one: https://www.waveshare.com/13.3inch-HDMI-LCD-H-with-case-V2.htm

We can connect two monitors to IMX8QXP (via USB type C to 4 USB 3.0 Hub) and can use touch on both monitors (OS is Android Automotive 11).

3,623 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tranvanmau,

The touch screen works on MX8-DSI-OLED but for Android automotive you must check with professional services:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Regards

 

0 Kudos
Reply