IMX8 Quadmax MEK Android Automotive 11 touch input support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8 Quadmax MEK Android Automotive 11 touch input support

ソリューションへジャンプ
5,361件の閲覧回数
tranvanmau
Contributor II

Hello,

We plan to use 8QuadMax MEK and MX8-DSI-OLED1 touch screen for our R&D project. Android_automotive-11.0.0_1.1.0 is OS.
However, [android_automotive-11.0.0_1.1.0_docs, Android_Release_Notes.pdf, Table 2. Features] only says that for "UI (input)" USB mouse is supported.

What about touch input? Can we use touch screen of MX8-DSI-OLED1 as UI input on 8QuadMax MEK Android_automotive-11.0.0_1.1.0 release?

Could someone help us to answer this question?

ラベル(1)
0 件の賞賛
返信
1 解決策
5,336件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tranvanmau,

The touch screen works on MX8-DSI-OLED but for Android automotive you must check with professional services:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,327件の閲覧回数
tranvanmau
Contributor II

Hello Bio_TICFSL,

Thank you for your info, I understand it.

Best regards,

0 件の賞賛
返信
5,304件の閲覧回数
dzvernik_gk
Contributor I

Hello @tranvanmau ,

Did you figure out if the it's possible to use this touch screen (MX8-DSI-OLED1) with the Android Automotive 11 [android_automotive-11.0.0_1.1.0] and it's support out-of-the-box ? 

 

@Bio_TICFSL could you please advice on availability of the MX8-DSI-OLED1 with any distributor since we figured out that there is no availability, at lest not online ?

 

Thanks.

Kind Regards.

0 件の賞賛
返信
5,269件の閲覧回数
tranvanmau
Contributor II

Hello @dzvernik_gk,

I did not know it yet. I closed this thread because the question needs special support from NXP.

Anyway, MX8-DSI-OLED1 is considered to be small (5.48 inch) for our project, so we are thinking of other approaches.

May be some USB touch screens out there can be used (such as this one https://www.viewsonicglobal.com/public/products_download/user_guide/Display/TD1655/TD1655_UG_ENG.pdf...)

Best regards,

0 件の賞賛
返信
4,969件の閲覧回数
tranvanmau
Contributor II

We buy this one: https://www.waveshare.com/13.3inch-HDMI-LCD-H-with-case-V2.htm

We can connect two monitors to IMX8QXP (via USB type C to 4 USB 3.0 Hub) and can use touch on both monitors (OS is Android Automotive 11).

5,337件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello tranvanmau,

The touch screen works on MX8-DSI-OLED but for Android automotive you must check with professional services:

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Regards

 

0 件の賞賛
返信