IMX7D needs Pull down resistors on UART TX and RX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D needs Pull down resistors on UART TX and RX?

1,898 Views
jhonathan_silva
Contributor I

I am using RS232 on UART pins. I'd like to make sure the MCIMX7D5EVM10SD needs external pull down on these pins  (e.g, UART1_TXD) or the internal pull down is enough?

Labels (1)
1 Reply

1,795 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jhonathan

in general they are not needed.

If there is special need, internal pull down is enough.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------