IMX7D needs Pull down resistors on UART TX and RX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX7D needs Pull down resistors on UART TX and RX?

2,063件の閲覧回数
jhonathan_silva
Contributor I

I am using RS232 on UART pins. I'd like to make sure the MCIMX7D5EVM10SD needs external pull down on these pins  (e.g, UART1_TXD) or the internal pull down is enough?

ラベル(1)
タグ(3)
1 返信

1,960件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jhonathan

in general they are not needed.

If there is special need, internal pull down is enough.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------