IMX6ULL MFGTOOL Cannot Write System

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL MFGTOOL Cannot Write System

ソリューションへジャンプ
2,443件の閲覧回数
baijinlong
Contributor III

hi,

      we have a custom board same as iMX6ULLevk,Then by using Mfgtools flashed compiled images to NAND successfully.

      But at the booting time it is getting stop at "cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)" without any errors.

MFGTOOL failed after booting the kernel:

       pastedImage_1.png              

  we attached custom board logs.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,171件の閲覧回数
baijinlong
Contributor III

The problem has been found. This problem is a problem with the kernel image. Recompile the firmware/zImage on it. I estimate that the kernel version is inconsistent. The corresponding solutions are as follows:
Compile zImage of MFGTOOL tool configuration, ie imx_v7_mfg_defconfig configuration, generate zImage into
In the mfgtools/Profiles/Linux/OS Firmware/firmware/ directory, you can write it; in addition, you must correct the DDR data and DDR stress test.   

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,172件の閲覧回数
baijinlong
Contributor III

The problem has been found. This problem is a problem with the kernel image. Recompile the firmware/zImage on it. I estimate that the kernel version is inconsistent. The corresponding solutions are as follows:
Compile zImage of MFGTOOL tool configuration, ie imx_v7_mfg_defconfig configuration, generate zImage into
In the mfgtools/Profiles/Linux/OS Firmware/firmware/ directory, you can write it; in addition, you must correct the DDR data and DDR stress test.   

0 件の賞賛
返信