IMX6ULL-MCIMX6Y2CVM08AA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6ULL-MCIMX6Y2CVM08AA

2,021件の閲覧回数
baijinlong
Contributor III

               The EMMC clock CLK level is abnormal. Under normal conditions, it is 3.3v level. However, after measurement, it is found that the EMMC clock CLK voltage is always 1.8v. What is the situation? Hope to get your help, thank you!

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,400件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jinlong

one can check power supplies of eMMC signals with oscilloscope, if they are changing in

application, please look at Table 91. 14 x 14 mm Functional Contact Assignments for "Power Group"

i.MX6ULL Datasheet
https://www.nxp.com/docs/en/data-sheet/IMX6ULLCEC.pdf 

and check power supplies using Design Checklist

https://www.nxp.com/docs/en/user-guide/IMX6ULLHDG.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信