IMX6ULL MFGTOOL Cannot Write System

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6ULL MFGTOOL Cannot Write System

跳至解决方案
2,492 次查看
baijinlong
Contributor III

hi,

      we have a custom board same as iMX6ULLevk,Then by using Mfgtools flashed compiled images to NAND successfully.

      But at the booting time it is getting stop at "cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)" without any errors.

MFGTOOL failed after booting the kernel:

       pastedImage_1.png              

  we attached custom board logs.

标签 (2)
0 项奖励
回复
1 解答
2,220 次查看
baijinlong
Contributor III

The problem has been found. This problem is a problem with the kernel image. Recompile the firmware/zImage on it. I estimate that the kernel version is inconsistent. The corresponding solutions are as follows:
Compile zImage of MFGTOOL tool configuration, ie imx_v7_mfg_defconfig configuration, generate zImage into
In the mfgtools/Profiles/Linux/OS Firmware/firmware/ directory, you can write it; in addition, you must correct the DDR data and DDR stress test.   

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,221 次查看
baijinlong
Contributor III

The problem has been found. This problem is a problem with the kernel image. Recompile the firmware/zImage on it. I estimate that the kernel version is inconsistent. The corresponding solutions are as follows:
Compile zImage of MFGTOOL tool configuration, ie imx_v7_mfg_defconfig configuration, generate zImage into
In the mfgtools/Profiles/Linux/OS Firmware/firmware/ directory, you can write it; in addition, you must correct the DDR data and DDR stress test.   

0 项奖励
回复