IMX6ULL Datasheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
14,953件の閲覧回数
umasundaram
Contributor II

Hi,

  We are designing a consumer product with IMX6UL processor.We would also like to use IMX6ULL processor as a drop-in replacement for IMX6UL, in our future PCB builds.

   Can you please provide clarification on the following.

Q1. What are the differences between  IMX6UL and IMX6ULL ,that needs to be considered in processor interface.Any design documents on IMX6ULL would be much appreciated.

Q2. Can you please provide us the datasheet/Reference manual/Hardware design guide of IMX6ULL. Only EVK design files are available for IMX6ULL.

Thanks,

Uma

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
9,071件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  Please use i.MX 6ULL Migration Guide :


http://www.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf
 

Also, please visit the following documentation Web :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

IMX6ULL Summary Page :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

6 返答(返信)
9,071件の閲覧回数
krunalshah
Contributor I

Hi Uma,

We have designed one system using imx6 UL and wants to upgrade to the imx6ULL, did you tried imx6ull replacement of imx6ul version? Do we need to do any changes in hardware/PCB?

Thanks

Krunal Shah

0 件の賞賛
返信
9,071件の閲覧回数
umasundaram
Contributor II

Hi Yuri,

  Thanks for the update.

Regards,

Uma

0 件の賞賛
返信
9,071件の閲覧回数
umasundaram
Contributor II

Thanks for the resources link.

   Can you please confirm the function of  pin "R15",of iMX6ULL.

Q1: Is it assigned to power "VDD_HIGH_CAP" or any other pins.

   Please find the image on Pg126 of IMX6ULL (Industrial grade) with R15 mentioned as "VDD_HIGH_CAP2".

pastedImage_1.png

 At page 115 of the datasheet,R15 is not assigned to any of the pins.

pastedImage_2.png

Thanks,

Uma

0 件の賞賛
返信
9,071件の閲覧回数
umasundaram
Contributor II

Hi all,

 Can you please let us know is there any update on the  above IMx6ULL pin clarification.

Thanks,

Uma.

0 件の賞賛
返信
9,071件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  There are two pins VDD_HIGH_CAP (R14) and VDD_HIGH_CAP2(R15), that must

be tied together (and named VDD_HIGH_CAP). The doc team is informed about it.

   Also, please refer to the i.MX6ULL EVK design.

MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP  

Regards,

Yuri.

0 件の賞賛
返信
9,072件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  Please use i.MX 6ULL Migration Guide :


http://www.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf
 

Also, please visit the following documentation Web :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

IMX6ULL Summary Page :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------