IMX6ULL Datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6ULL Datasheet

跳至解决方案
15,137 次查看
umasundaram
Contributor II

Hi,

  We are designing a consumer product with IMX6UL processor.We would also like to use IMX6ULL processor as a drop-in replacement for IMX6UL, in our future PCB builds.

   Can you please provide clarification on the following.

Q1. What are the differences between  IMX6UL and IMX6ULL ,that needs to be considered in processor interface.Any design documents on IMX6ULL would be much appreciated.

Q2. Can you please provide us the datasheet/Reference manual/Hardware design guide of IMX6ULL. Only EVK design files are available for IMX6ULL.

Thanks,

Uma

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
9,255 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please use i.MX 6ULL Migration Guide :


http://www.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf
 

Also, please visit the following documentation Web :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

IMX6ULL Summary Page :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

6 回复数
9,255 次查看
krunalshah
Contributor I

Hi Uma,

We have designed one system using imx6 UL and wants to upgrade to the imx6ULL, did you tried imx6ull replacement of imx6ul version? Do we need to do any changes in hardware/PCB?

Thanks

Krunal Shah

0 项奖励
回复
9,255 次查看
umasundaram
Contributor II

Hi Yuri,

  Thanks for the update.

Regards,

Uma

0 项奖励
回复
9,255 次查看
umasundaram
Contributor II

Thanks for the resources link.

   Can you please confirm the function of  pin "R15",of iMX6ULL.

Q1: Is it assigned to power "VDD_HIGH_CAP" or any other pins.

   Please find the image on Pg126 of IMX6ULL (Industrial grade) with R15 mentioned as "VDD_HIGH_CAP2".

pastedImage_1.png

 At page 115 of the datasheet,R15 is not assigned to any of the pins.

pastedImage_2.png

Thanks,

Uma

0 项奖励
回复
9,255 次查看
umasundaram
Contributor II

Hi all,

 Can you please let us know is there any update on the  above IMx6ULL pin clarification.

Thanks,

Uma.

0 项奖励
回复
9,255 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  There are two pins VDD_HIGH_CAP (R14) and VDD_HIGH_CAP2(R15), that must

be tied together (and named VDD_HIGH_CAP). The doc team is informed about it.

   Also, please refer to the i.MX6ULL EVK design.

MCIMX6ULL-EVK|i.MX6ULL Evaluation Kit|NXP  

Regards,

Yuri.

0 项奖励
回复
9,256 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please use i.MX 6ULL Migration Guide :


http://www.nxp.com/assets/documents/data/en/application-notes/AN5350.pdf
 

Also, please visit the following documentation Web :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

IMX6ULL Summary Page :

i.MX 6ULL Applications Processor | ARM Cortex-A7|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------