IMX6Q cpu rcu error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q cpu rcu error

3,476 Views
ivychend
Contributor I

hello, community

         I have met the error for many times atfer hours of playing video through video app. The error leads to two problems:

1    The kenrel crash may cause serious problem of out product in the furture, that is what we do not want see. 

2    The error make the video app recognise network as not working. But when I refresh the video app, it still can play network video. and I can ping an internet IP. So it means that the network work fine, but the video app recognise not

What cause this error happens or how to fix it ?  Any answer will be appriciated.

error log follows

error log:

root@sabresd_6dq:/ # [11046.548509] INFO: rcu_bh_state detected stall on CPU 3 (t=0 jiffies)
[11046.555031] Backtrace for cpu 3 (current):
[11046.559436] [<c00b1a04>] (unwind_backtrace+0x0/0x138) from [<c00b0888>] (smp_send_all_cpu_backtrace+0x60/0xdc)
[11046.569633] [<c00b0888>] (smp_send_all_cpu_backtrace+0x60/0xdc) from [<c0132758>] (__rcu_pending+0x144/0x3c0)
[11046.579849] [<c0132758>] (__rcu_pending+0x144/0x3c0) from [<c01332e4>] (rcu_check_callbacks+0x11c/0x204)
[11046.589630] [<c01332e4>] (rcu_check_callbacks+0x11c/0x204) from [<c00f7974>] (update_process_times+0x38/0x68)
[11046.599850] [<c00f7974>] (update_process_times+0x38/0x68) from [<c0116f5c>] (tick_sched_timer+0x80/0xe4)
[11046.609633] [<c0116f5c>] (tick_sched_timer+0x80/0xe4) from [<c010a9d4>] (__run_hrtimer+0x80/0x2c0)
[11046.618888] [<c010a9d4>] (__run_hrtimer+0x80/0x2c0) from [<c010b8d0>] (hrtimer_interrupt+0x118/0x294)
[11046.628404] [<c010b8d0>] (hrtimer_interrupt+0x118/0x294) from [<c00a4320>] (do_IPI+0x14c/0x208)
[11046.637284] [<c00a4320>] (do_IPI+0x14c/0x208) from [<c00aa34c>] (__irq_svc+0x4c/0xe8)
[11046.645391] Exception stack(0xd609bf90 to 0xd609bfd8)
[11046.650595] bf80: c0999ae8 600a0093 00000001 00000000
[11046.659052] bfa0: d609a000 c0985684 c091ba6c c06abd44 c0924234 412fc09a 00000000 00000000
[11046.667515] bfc0: 00000000 d609bfd8 c00b9ba4 c00ab468 400a0013 ffffffff
[11046.674426] [<c00aa34c>] (__irq_svc+0x4c/0xe8) from [<c00ab468>] (default_idle+0x24/0x28)
[11046.682771] [<c00ab468>] (default_idle+0x24/0x28) from [<c00ab790>] (cpu_idle+0xe0/0x124)
[11046.691081] [<c00ab790>] (cpu_idle+0xe0/0x124) from [<1069e494>] (0x1069e494)
[11046.698332]
[11046.698335] sending IPI to all other CPUs:
[11046.704046] IPI backtrace for cpu 2
[11046.707601]
[11046.709211] Pid: 1278, comm: kinteractiveup
[11046.713979] CPU: 2 Not tainted (3.0.35 #299)
[11046.718669] PC is at generic_exec_single+0x6c/0x90
[11046.723580] LR is at arch_send_call_function_single_ipi+0x34/0x38
[11046.729738] pc : [<c011bbb4>] lr : [<c00b068c>] psr: 20000013
[11046.729743] sp : d67e3e28 ip : 00000000 fp : c091c7d0
[11046.741404] r10: 00000001 r9 : c28a1888 r8 : 027fe000
[11046.746745] r7 : c28a1880 r6 : 00000003 r5 : c28a1880 r4 : d67e3e54
[11046.753335] r3 : 00000001 r2 : f2a01000 r1 : 00000005 r0 : c06abcc8
[11046.759980] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[11046.767407] Control: 10c53c7d Table: 2386c04a DAC: 00000015
[11046.773214]
[11046.773216] PC: 0xc011bb34:
[11046.777615] bb34 e59f0008 e3a01079 ebff3213 eafffff6 c0813938 e59f3080 e92d47f0 e1a06000
[11046.786562] bb54 e7938100 e1a04001 e59f5070 e1a0a002 e0857008 e2879008 e1a00009 eb163607
[11046.795515] bb74 e5973004 e7955008 e5874004 e5847000 e5843004 e5834000 e1a01000 e1a00009
[11046.804458] bb94 eb1634af e1570005 0a000008 e35a0000 08bd87f0 e1d431b0 e3130001 08bd87f0
[11046.813348] bbb4 e1d431b0 e3130001 1afffffc e8bd87f0 e1a00006 ebfe52a2 eafffff3 c091c7d0
[11046.822288] bbd4 c00a3880 e92d45f0 e24dd024 e1a05000 e1a06001 e1a0c00d e3cc4d7f e3c4403f
[11046.831232] bbf4 e3a0c000 e58dc010 e58dc00c e5947004 e58dc014 e58dc018 e2877001 e58dc01c
[11046.840179] bc14 e5847004 e5947014 e59f8168 e3570000 e287c01f e207101f a1a0c007 e5980000
[11046.849070]
[11046.849072] LR: 0xc00b060c:
[11046.853527] 060c e59f0020 e1a01004 e8bd4010 ea17c6fd e59f0014 e1a01004 e8bd4010 ea17c6f9
[11046.862415] 062c c09245c4 c0807d74 c0807d88 c0807d58 e92d4008 e3053818 e34c3098 e3a01004
[11046.871364] 064c e5933000 e12fff33 e8bd8008 e200201f e30b1cb8 e2822001 e34c106a e92d4008
[11046.880312] 066c e0812102 e3053818 e1a002a0 e34c3098 e3a01005 e0420100 e5933000 e12fff33
[11046.889264] 068c e8bd8008 e59f3098 e92d4ff0 e241b001 e59f9090 e24dd00c e59f708c e1a06000
[11046.898156] 06ac e593a000 e3a05000 e59f8080 e1a00006 e59f107c e1a0200b e59f3078 e58d5000
[11046.907096] 06cc e3e04000 eb03ddb0 ea000001 e5922008 eb03ddad e2842001 e3a01004 e1a0000a
[11046.916040] 06ec eb09382b e59f1050 e0853180 e1a04000 e1a00006 e0882103 e5973000 e1530004
[11046.924930]
[11046.924932] SP: 0xd67e3da8:
[11046.929385] 3da8 d67e3de0 c0985818 c091c7d0 c00abbf0 c091c7d0 c00a436c ffffffff f2a00100
[11046.938330] 3dc8 00000c07 00000002 00000001 d67e2000 00000001 c00aa34c c06abcc8 00000005
[11046.947217] 3de8 f2a01000 00000001 d67e3e54 c28a1880 00000003 c28a1880 027fe000 c28a1888
[11046.956161] 3e08 00000001 c091c7d0 00000000 d67e3e28 c00b068c c011bbb4 20000013 ffffffff
[11046.965107] 3e28 d67e2000 00000000 c00b11b8 00000002 c06abd44 d67e3f28 d67e3f28 c011bcf0
[11046.973999] 3e48 d6191600 d6191600 80002001 c28a1880 c28a1880 c00b11b8 00000000 00000001
[11046.982942] 3e68 d67e69a0 ffffffff c095cbcc 00000000 d67e3f28 00000001 d67e3f28 c00b1330
[11046.991888] 3e88 c00b12e8 c010c798 c09e7acc c09e7ab4 00000000 00000001 ffffffff c010c8ec
[11047.000832]
[11047.000834] FP: 0xc091c750:
[11047.005235] c750 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.014174] c770 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.023061] c790 00000064 00008000 0000000f c28a7020 00000008 00000004 c28a7000 c289f000
[11047.032006] c7b0 c2888000 0000002c c288f000 c2897000 00000001 00001000 00000000 00000003
[11047.040952] c7d0 027e6000 027ee000 027f6000 027fe000 00057700 00000002 00028ffb 0008ffff
[11047.049897] c7f0 00000001 00000032 0000fffa 00000001 d6491ae0 d6491a80 00000000 d6018f20
[11047.058786] c810 0000000f d601d580 d6491a20 d6000a20 00000010 c28a9120 0000ffff 00000064
[11047.067669] c830 d6000a80 0000000f c28e9120 00007fff d6018f80 00100000 d601b000 0000000f
[11047.076609]
[11047.076611] R0: 0xc06abc48:
[11047.081010] bc48 55062042 20440720 09204108 430a2057 20490b20 73756170 6e6f5f65 706f6f5f
[11047.089949] bc68 00000073 696e6170 00000063 423e323c 203a4755 65636572 7020746e 746e6972
[11047.098887] bc88 6572206b 73727563 216e6f69 0000000a 6e697270 742e6b74 00656d69 7570635f
[11047.107771] bca8 0070755f 7570635f 776f645f 0000006e 00000000 00000001 00000002 00000004
[11047.116661] bcc8 00000008 00000010 00000020 00000040 00000080 00000100 00000200 00000400
[11047.125600] bce8 00000800 00001000 00002000 00004000 00008000 00010000 00020000 00040000
[11047.134544] bd08 00080000 00100000 00200000 00400000 00800000 01000000 02000000 04000000
[11047.143428] bd28 08000000 10000000 20000000 40000000 80000000 c091bb20 c091bb18 c091bb14
[11047.152370]
[11047.152372] R2: 0xf2a00f80:
[11047.156772] 0f80 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.165655] 0fa0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.174593] 0fc0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.183539] 0fe0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.192424] 1000 00000001 0000fc64 0102043b 00000000 00000000 00000000 00000000 00000000
[11047.201367] 1020 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.210306] 1040 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.219195] 1060 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.228140]
[11047.228142] R4: 0xd67e3dd4:
[11047.232595] 3dd4 d67e2000 00000001 c00aa34c c06abcc8 00000005 f2a01000 00000001 d67e3e54
[11047.241490] 3df4 c28a1880 00000003 c28a1880 027fe000 c28a1888 00000001 c091c7d0 00000000
[11047.250435] 3e14 d67e3e28 c00b068c c011bbb4 20000013 ffffffff d67e2000 00000000 c00b11b8
[11047.259376] 3e34 00000002 c06abd44 d67e3f28 d67e3f28 c011bcf0 d6191600 d6191600 80002001
[11047.268267] 3e54 c28a1880 c28a1880 c00b11b8 00000000 00000001 d67e69a0 ffffffff c095cbcc
[11047.277211] 3e74 00000000 d67e3f28 00000001 d67e3f28 c00b1330 c00b12e8 c010c798 c09e7acc
[11047.286157] 3e94 c09e7ab4 00000000 00000001 ffffffff c010c8ec 00000000 c0985eb4 001312d0
[11047.295102] 3eb4 d67e3f28 00000001 d62918e0 000f32a0 c097d2e8 00000003 c010c920 00000000
[11047.303990]
[11047.303992] R5: 0xc28a1800:
[11047.308444] 1800 6c0f8f37 000001a8 000002a1 00000000 00fec563 005d903b 007dd145 005e39a8
[11047.317337] 1820 d6143a40 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.326289] 1840 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.335231] 1860 c09080e0 00200200 c00b8160 00000000 00000000 00000000 00000000 00000000
[11047.344173] 1880 d67e3e54 d67e3e54 00000000 00000000 00000000 00000000 00000000 00000000
[11047.353064] 18a0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.362006] 18c0 00000000 c28a18c0 c28a18c8 c28a18c8 00000000 c28a18d4 c28a18d4 00000000
[11047.370897] 18e0 00000000 00000000 0000a816 00000000 00000000 00000000 00000000 00000000
[11047.379839]
[11047.379841] R7: 0xc28a1800:
[11047.384241] 1800 6c0f8f37 000001a8 000002a1 00000000 00fec563 005d903b 007dd145 005e39a8
[11047.393187] 1820 d6143a40 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.402084] 1840 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.411031] 1860 c09080e0 00200200 c00b8160 00000000 00000000 00000000 00000000 00000000
[11047.419921] 1880 d67e3e54 d67e3e54 00000000 00000000 00000000 00000000 00000000 00000000
[11047.428864] 18a0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.437755] 18c0 00000000 c28a18c0 c28a18c8 c28a18c8 00000000 c28a18d4 c28a18d4 00000000
[11047.446702] 18e0 00000000 00000000 0000a816 00000000 00000000 00000000 00000000 00000000
[11047.455640]
[11047.455642] R9: 0xc28a1808:
[11047.460041] 1808 000002a1 00000000 00fec563 005d903b 007dd145 005e39a8 d6143a40 00000000
[11047.468930] 1828 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.477877] 1848 00000000 00000000 00000000 00000000 00000000 00000000 c09080e0 00200200
[11047.486766] 1868 c00b8160 00000000 00000000 00000000 00000000 00000000 d67e3e54 d67e3e54
[11047.495706] 1888 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.504639] 18a8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 c28a18c0
[11047.513523] 18c8 c28a18c8 c28a18c8 00000000 c28a18d4 c28a18d4 00000000 00000000 00000000
[11047.522464] 18e8 0000a816 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.531411] IPI backtrace for cpu 0
[11047.534963]
[11047.536516] Pid: 0, comm: swapper
[11047.541075] CPU: 0 Not tainted (3.0.35 #299)
[11047.545761] PC is at default_idle+0x24/0x28
[11047.550012] LR is at arch_idle+0xbc/0xf4
[11047.554054] pc : [<c00ab468>] lr : [<c00b9ba4>] psr: 40000013
[11047.554059] sp : c0907fb0 ip : 00000000 fp : 00000000
[11047.565724] r10: 00000000 r9 : 412fc09a r8 : c0924234
[11047.571012] r7 : c06abd44 r6 : c091ba6c r5 : c0985684 r4 : c0906000
[11047.577658] r3 : 00000000 r2 : 00000001 r1 : 20000093 r0 : c0999ae8
[11047.584250] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[11047.591677] Control: 10c53c7d Table: 2386c04a DAC: 00000015
[11047.597539]
[11047.597541] PC: 0xc00ab3e8:
[11047.601942] b3e8 c09739b8 c0806880 c06aa37c c08068a0 e121f007 e1a00004 e1a0e006 e1a0f005
[11047.610898] b408 eb01015c e320f000 e3053684 e34c3098 e5932000 e2822001 e5832000 e12fff1e
[11047.619796] b428 e3053684 e34c3098 e5932000 e2422001 e5832000 e12fff1e e12fff1e e92d4008
[11047.628754] b448 e1a0200d e3c23d7f e3c3303f e5933000 e3130002 1a000000 eb0039a0 f1080080
[11047.637706] b468 e8bd8008 e92d4070 e24dd050 e1a04000 e1a05001 e28d0008 e3a01048 e1a06002
[11047.646658] b488 eb095134 e3a0c000 e3860502 e1a0100c e28d2008 e1a0300c e3800c01 e58d5018
[11047.655551] b4a8 e30be408 e58d401c e34ce00a e58dc000 e58de020 e3a0e013 e58dc004 e58de024
[11047.664504] b4c8 e30be3f8 e34ce00a e58de044 e3a0e093 e58de048 eb00f016 e28dd050 e8bd8070
[11047.673463]
[11047.673465] LR: 0xc00b9b24:
[11047.677868] 9b24 e8bd8000 ebfffe9b ebffff44 eafffffa eb017426 e3500000 0afffff7 e3a00004
[11047.686823] 9b44 e08d1000 eb016ccc e59f307c e5d33010 e3530000 13a00000 03a00002 ebfffe8d
[11047.695772] 9b64 e59f3068 e5d33000 e3530000 1a00000e e59f305c e5933000 e5930000 e200000f
[11047.704669] 9b84 eb0956ee e3500001 0a000005 e59d0004 ebffffbc e3a00005 e28d1004 eb016cb6
[11047.713699] 9ba4 eaffffdd ebffff2f eafffff9 e3a03901 e34f340c e5932064 e3c22002 e5832064
[11047.722651] 9bc4 ebffff1e eafffff2 c0924c58 c0985a48 c0985a30 c06abd48 e3a03902 e340320d
[11047.731552] 9be4 e5932040 e3822030 e5832040 e5932044 e3822201 e5832044 e12fff1e e3a03902
[11047.740442] 9c04 e340320d e5932040 e3c22030 e5832040 e5932044 e3c22201 e5832044 e12fff1e
[11047.749396]
[11047.749398] SP: 0xc0907f30:
[11047.753800] 7f30 c0907f68 c0985818 00000000 c00abbf0 c091c7d0 c00a436c ffffffff f2a00100
[11047.762754] 7f50 00000c07 00000002 00000001 c0906000 00000000 c00aa34c c0999ae8 20000093
[11047.771706] 7f70 00000001 00000000 c0906000 c0985684 c091ba6c c06abd44 c0924234 412fc09a
[11047.780604] 7f90 00000000 00000000 00000000 c0907fb0 c00b9ba4 c00ab468 40000013 ffffffff
[11047.789500] 7fb0 c00ab444 c00ab790 c091c61c 00000000 c0036664 c28851c0 1000406a c00088bc
[11047.798456] 7fd0 c00082f8 00000000 00000000 c0036664 00000000 10c53c7d c091ba8c c0036660
[11047.807408] 7ff0 c092422c 10008040 00000000 00000000 00000000 00000000 00000000 00000000
[11047.816301] 8010 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.825252]
[11047.825254] R0: 0xc0999a68:
[11047.829708] 9a68 00000000 00000000 00000000 00000000 00000000 00000000 c0111e80 c2888530
[11047.838606] 9a88 00000000 ffffffff 00000000 00000000 00000000 00000000 00000000 00000000
[11047.847552] 9aa8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.856502] 9ac8 00000000 00000000 00000000 00000000 00000000 00000000 d60090c0 00000001
[11047.865397] 9ae8 00000000 00000000 c0933918 00000000 37ad7580 00000a0c 00989680 00000000
[11047.874350] 9b08 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.883304] 9b28 c092fbc0 00000001 00000000 00000000 00000000 00000000 38460c00 00000a0c
[11047.892257] 9b48 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.901160]
[11047.901162] R4: 0xc0905f80:
[11047.905619] 5f80 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.914518] 5fa0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.923466] 5fc0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.932423] 5fe0 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.941375] 6000 00000000 00000004 00000000 c0923030 c0931114 00000000 00000015 c0923030
[11047.950276] 6020 c2889320 d2229860 c0906000 48d967d8 d2dc00c0 00000000 c0907fb4 c0907f00
[11047.959228] 6040 c06a6a70 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.968181] 6060 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.977076]
[11047.977078] R5: 0xc0985604:
[11047.981482] 5604 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.990439] 5624 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11047.999336] 5644 00000000 00000000 00000000 00000000 0007a25b 00000000 00000001 00000000
[11048.008284] 5664 00000000 00000000 00000000 00000000 00000003 00000000 00000000 00000000
[11048.017230] 5684 00000000 c00c892c 00000000 00000000 c0923eec 00000000 00000000 e31698f4
[11048.026124] 56a4 1e1919d4 00063015 c00b841c 006c3776 00000000 c080b608 00000000 c0999ae8
[11048.035025] 56c4 c00ab468 40000013 00000000 401bee34 600e0010 84317310 402005c8 800e0010
[11048.043982] 56e4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 c0999ae8
[11048.052933]
[11048.052935] R6: 0xc091b9ec:
[11048.057336] b9ec 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.066290] ba0c 00000000 00000000 00000000 00000000 00000000 00000001 00000000 0000b0d7
[11048.075188] ba2c c00b82b0 c00b82f0 c0780000 c00b8040 c00b7fec c00b7d80 c00b7e2c c00b7e44
[11048.084092] ba4c c00b7e44 c00b7e48 c00b7e48 c00b7ecc c00b7fc4 c00b7fd4 c00b7f8c 00000012
[11048.093047] ba6c c00b8598 c00b86f8 c00b864c c00b8528 c00b87cc c00b84e0 c00b8568 00000000
[11048.101999] ba8c 00000f8c 00000000 f2a01000 f2a00100 f2a00100 000003e8 00000000 00003c6f
[11048.110905] baac 00000001 c080f214 c080f22c c080f238 c080f248 c080f258 c080f264 c080f270
[11048.119864] bacc c080f280 c080f28c c080f294 c080f2a0 c080f2a8 c080f2b4 c080f2c4 c080f2d0
[11048.128765]
[11048.128767] R7: 0xc06abcc4:
[11048.133167] bcc4 00000004 00000008 00000010 00000020 00000040 00000080 00000100 00000200
[11048.142124] bce4 00000400 00000800 00001000 00002000 00004000 00008000 00010000 00020000
[11048.151078] bd04 00040000 00080000 00100000 00200000 00400000 00800000 01000000 02000000
[11048.159978] bd24 04000000 08000000 10000000 20000000 40000000 80000000 c091bb20 c091bb18
[11048.168932] bd44 c091bb14 c091bb1c 0000000f 00000000 c080fb50 00000001 c080fb54 00000002
[11048.177833] bd64 c080fb5c 00000003 c080fb64 00000004 c080fb6c 00000005 c080fb74 00000006
[11048.186787] bd84 c080fb84 00000007 c080fb8c 00000008 c080fb94 00000009 c080fb9c ffffffff
[11048.195686] bda4 00000000 00000063 63657622 2075253d 7463615b 3d6e6f69 225d7325 4552202c
[11048.204637]
[11048.204639] R8: 0xc09241b4:
[11048.209040] 41b4 00000000 c00a9624 00000000 c00a94d4 00000000 c00a945c 00000000 c00a9434
[11048.218001] 41d4 00000000 c00a90d4 00000000 c00a8f5c 00000000 c00a8884 00000000 00000000
[11048.226905] 41f4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.235862] 4214 00000000 00000000 00000000 00000000 00000000 c00aa800 10c53c7d 10c53c7d
[11048.244765] 4234 00000068 c00ab444 c00ab53c c092433c c092425c 0fffffff 07f001f0 00000020
[11048.253719] 4254 00000000 c00ac668 c0924240 c0924278 0000ffff 0000de01 00000020 00000020
[11048.262674] 4274 c00ac668 c092425c c092433c 0000ffff 0000f7f0 00000020 00000020 c00ac610
[11048.271574] 4294 00000000 00000000 c080709c 00000200 00000000 00000000 00000000 100a4000
[11048.280532] IPI backtrace for cpu 1
[11048.284140]
[11048.285696] Pid: 0, comm: swapper
[11048.290209] CPU: 1 Not tainted (3.0.35 #299)
[11048.294897] PC is at default_idle+0x24/0x28
[11048.299204] LR is at arch_idle+0xbc/0xf4
[11048.303191] pc : [<c00ab468>] lr : [<c00b9ba4>] psr: 400b0013
[11048.303195] sp : d6065fd8 ip : 00000000 fp : 00000000
[11048.314860] r10: 00000000 r9 : 412fc09a r8 : c0924234
[11048.320203] r7 : c06abd44 r6 : c091ba6c r5 : c0985684 r4 : d6064000
[11048.326792] r3 : 00000000 r2 : 00000001 r1 : 600b0093 r0 : c0999ae8
[11048.333435] Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[11048.340809] Control: 10c53c7d Table: 220c804a DAC: 00000015
[11048.346672]
[11048.346674] PC: 0xc00ab3e8:
[11048.351074] b3e8 c09739b8 c0806880 c06aa37c c08068a0 e121f007 e1a00004 e1a0e006 e1a0f005
[11048.360035] b408 eb01015c e320f000 e3053684 e34c3098 e5932000 e2822001 e5832000 e12fff1e
[11048.369005] b428 e3053684 e34c3098 e5932000 e2422001 e5832000 e12fff1e e12fff1e e92d4008
[11048.377920] b448 e1a0200d e3c23d7f e3c3303f e5933000 e3130002 1a000000 eb0039a0 f1080080
[11048.386887] b468 e8bd8008 e92d4070 e24dd050 e1a04000 e1a05001 e28d0008 e3a01048 e1a06002
[11048.395838] b488 eb095134 e3a0c000 e3860502 e1a0100c e28d2008 e1a0300c e3800c01 e58d5018
[11048.404787] b4a8 e30be408 e58d401c e34ce00a e58dc000 e58de020 e3a0e013 e58dc004 e58de024
[11048.413685] b4c8 e30be3f8 e34ce00a e58de044 e3a0e093 e58de048 eb00f016 e28dd050 e8bd8070
[11048.422637]
[11048.422639] LR: 0xc00b9b24:
[11048.427039] 9b24 e8bd8000 ebfffe9b ebffff44 eafffffa eb017426 e3500000 0afffff7 e3a00004
[11048.435988] 9b44 e08d1000 eb016ccc e59f307c e5d33010 e3530000 13a00000 03a00002 ebfffe8d
[11048.444939] 9b64 e59f3068 e5d33000 e3530000 1a00000e e59f305c e5933000 e5930000 e200000f
[11048.453890] 9b84 eb0956ee e3500001 0a000005 e59d0004 ebffffbc e3a00005 e28d1004 eb016cb6
[11048.462782] 9ba4 eaffffdd ebffff2f eafffff9 e3a03901 e34f340c e5932064 e3c22002 e5832064
[11048.471726] 9bc4 ebffff1e eafffff2 c0924c58 c0985a48 c0985a30 c06abd48 e3a03902 e340320d
[11048.480677] 9be4 e5932040 e3822030 e5832040 e5932044 e3822201 e5832044 e12fff1e e3a03902
[11048.489581] 9c04 e340320d e5932040 e3c22030 e5832040 e5932044 e3c22201 e5832044 e12fff1e
[11048.498480]
[11048.498482] SP: 0xd6065f58:
[11048.502937] 5f58 d6065f90 c0985818 00000000 c00abbf0 c091c7d0 c00a436c ffffffff f2a00100
[11048.511831] 5f78 00000c07 00000002 00000001 d6064000 00000000 c00aa34c c0999ae8 600b0093
[11048.520777] 5f98 00000001 00000000 d6064000 c0985684 c091ba6c c06abd44 c0924234 412fc09a
[11048.529726] 5fb8 00000000 00000000 00000000 d6065fd8 c00b9ba4 c00ab468 400b0013 ffffffff
[11048.538615] 5fd8 c00ab444 c00ab790 2350c06a 00000015 10c03c7d c0985820 1000406a 1069e494
[11048.547510] 5ff8 ffffffff ffffffff eed40000 bac22d07 6acf79cc 000844b1 38040045 00400000
[11048.556461] 6018 5dc71140 7701a8c0 6c33cc79 47074707 248d2404 428819fe 79cc0024 44b16acf
[11048.565411] 6038 2d07eed4 eed4bac2 bac22d07 0000df50 79cc62f1 44b16acf 2d07eed4 0008bac2
[11048.574314]
[11048.574316] R0: 0xc0999a68:
[11048.578772] 9a68 00000000 00000000 00000000 00000000 00000000 00000000 c0111e80 c2888530
[11048.587669] 9a88 00000000 ffffffff 00000000 00000000 00000000 00000000 00000000 00000000
[11048.596565] 9aa8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.605511] 9ac8 00000000 00000000 00000000 00000000 00000000 00000000 d60090c0 00000001
[11048.614456] 9ae8 00000000 00000000 c0933918 00000000 64618d00 00000a0c 00989680 00000000
[11048.623354] 9b08 00000000 00000000 00000000 00000000 00000000 00000000 00000001 00000000
[11048.632307] 9b28 c092fbc0 00000001 00000000 00000000 00000000 00000000 64fa2380 00000a0c
[11048.641254] 9b48 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.650197]
[11048.650199] R4: 0xd6063f80:
[11048.654602] 3f80 65755165 00000005 62138aa8 62138a98 fffffffc 000000f0 c00aaa84 00000000
[11048.663549] 3fa0 41b04228 c00aa900 62138aa8 62138a98 62138aa8 00000080 fffffffc 00000000
[11048.672444] 3fc0 62138aa8 62138a98 fffffffc 000000f0 00000000 00000000 00000000 41b04228
[11048.681396] 3fe0 00000000 755e7bc8 401ecfa0 401ffa00 60070010 62138aa8 e9c934b6 2131f997
[11048.690348] 4000 00000002 00000004 00000000 d6044560 c0931114 00000001 00000015 d6044560
[11048.699291] 4020 c2891320 d69acdc0 d6064000 c00a21b4 d618c600 00000001 d6065fdc d6065f28
[11048.708186] 4040 c06a6a70 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.717138] 4060 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.726087]
[11048.726089] R5: 0xc0985604:
[11048.730490] 5604 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.739447] 5624 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.748407] 5644 00000000 00000000 00000000 00000000 0007a25b 00000000 00000001 00000000
[11048.757309] 5664 00000000 00000000 00000000 00000000 00000003 00000000 00000000 00000000
[11048.766273] 5684 00000000 c00c892c 00000000 00000000 c0923eec 00000000 00000000 e31698f4
[11048.775225] 56a4 1e1919d4 00063015 c00b841c 006c3776 00000000 c080b608 00000000 c0999ae8
[11048.784190] 56c4 c00ab468 40000013 4022c2f8 401ee48a 200a0030 7930fc08 402005c8 800a0010
[11048.793113] 56e4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 c0999ae8
[11048.802087]
[11048.802089] R6: 0xc091b9ec:
[11048.806496] b9ec 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.815474] ba0c 00000000 00000000 00000000 00000000 00000000 00000001 00000000 0000b0d7
[11048.824453] ba2c c00b82b0 c00b82f0 c0780000 c00b8040 c00b7fec c00b7d80 c00b7e2c c00b7e44
[11048.833425] ba4c c00b7e44 c00b7e48 c00b7e48 c00b7ecc c00b7fc4 c00b7fd4 c00b7f8c 00000012
[11048.842344] ba6c c00b8598 c00b86f8 c00b864c c00b8528 c00b87cc c00b84e0 c00b8568 00000000
[11048.851331] ba8c 00000f8c 00000000 f2a01000 f2a00100 f2a00100 000003e8 00000000 00003c6f
[11048.860306] baac 00000001 c080f214 c080f22c c080f238 c080f248 c080f258 c080f264 c080f270
[11048.869231] bacc c080f280 c080f28c c080f294 c080f2a0 c080f2a8 c080f2b4 c080f2c4 c080f2d0
[11048.878210]
[11048.878212] R7: 0xc06abcc4:
[11048.882675] bcc4 00000004 00000008 00000010 00000020 00000040 00000080 00000100 00000200
[11048.891599] bce4 00000400 00000800 00001000 00002000 00004000 00008000 00010000 00020000
[11048.900575] bd04 00040000 00080000 00100000 00200000 00400000 00800000 01000000 02000000
[11048.909551] bd24 04000000 08000000 10000000 20000000 40000000 80000000 c091bb20 c091bb18
[11048.918464] bd44 c091bb14 c091bb1c 0000000f 00000000 c080fb50 00000001 c080fb54 00000002
[11048.927436] bd64 c080fb5c 00000003 c080fb64 00000004 c080fb6c 00000005 c080fb74 00000006
[11048.936358] bd84 c080fb84 00000007 c080fb8c 00000008 c080fb94 00000009 c080fb9c ffffffff
[11048.945336] bda4 00000000 00000063 63657622 2075253d 7463615b 3d6e6f69 225d7325 4552202c
[11048.954257]
[11048.954259] R8: 0xc09241b4:
[11048.958722] 41b4 00000000 c00a9624 00000000 c00a94d4 00000000 c00a945c 00000000 c00a9434
[11048.967635] 41d4 00000000 c00a90d4 00000000 c00a8f5c 00000000 c00a8884 00000000 00000000
[11048.976619] 41f4 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[11048.985537] 4214 00000000 00000000 00000000 00000000 00000000 c00aa800 10c53c7d 10c53c7d
[11048.994511] 4234 00000068 c00ab444 c00ab53c c092433c c092425c 0fffffff 07f001f0 00000020
[11049.003432] 4254 00000000 c00ac668 c0924240 c0924278 0000ffff 0000de01 00000020 00000020
[11049.012409] 4274 c00ac668 c092425c c092433c 0000ffff 0000f7f0 00000020 00000020 c00ac610
[11049.021385] 4294 00000000 00000000 c080709c 00000200 00000000 00000000 00000000 100a4000
[26421.421736] binder: send failed reply for transaction 4576815 to 29330:29348

Labels (2)
0 Kudos
Reply
6 Replies

2,371 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

such kind of error were on older releases due to arm/gpu bugs

(just for test one can try to disable GPU). Please try latest L4.1.x nxp bsps

were most of these errata were fixed

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


================================================================
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,371 Views
ivychend
Contributor I

Hi, igor

Thanks for you answer, how to disable GPU. I have tried disable GPU(vivante driver) in kernel CONFIG, and then built kernel and burnt boot.img. But the board can not access android, just printed error log in the phase of init continuesly(like this kind error: init kill * pid, packed ***).

another question is that I am using imx6q android 4.4.2,  should I just replace kenrel with another version or replace the whole BSP with the  lastest version

0 Kudos
Reply

2,370 Views
igorpadykov
NXP Employee
NXP Employee

please try attached patch, in general recommended to move to latest Android BSPs on

i.MX 6 Series Software and Development Tool|NXP 

~igor

0 Kudos
Reply

2,370 Views
ivychend
Contributor I

igor

thanks

Have downloaded KitKat4.4.2_1.0.0-upgrade-gpu-to-latest-4.6.9p13-Ver6.zip and tried to patch to my source code manually( can not use patch command ). I found the patch do not match my source code version. For example

patch :

pastedImage_15.png

source code: kernel_imx\drivers\mxc\gpu-viv\arch\XAQ2\hal\kernel\gc_hal_kernel_hardware.c

pastedImage_16.png

gckHARDWARE_InitializeHardware  precise position:      This function was just called one time this file

pastedImage_17.png

so I wish to get the whole complete files, not just patch files. where can I get that

0 Kudos
Reply

2,370 Views
igorpadykov
NXP Employee
NXP Employee

for porting patches with old bsps may be recommended to apply to

NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Pro-Support contact www.nxp.com/prosupport

Best regards
igor

0 Kudos
Reply

2,370 Views
之金叶
Contributor I

dear ,my 6q,android4.4.2,have patched KfttKat4.4.2_1.0.0-upgrade-gpu-to-latest-4.6.9p13-Ver6.zip,but the issue also when paly music after 24 hours; log is as blow:

[20180129_22:33:21][28097.927490] ---[ end trace 72c965a0ff309782 ]---
[20180129_22:40:53][28549.634032] INFO: rcu_bh_state detected stall on CPU 2 (t=0 jiffies)
[20180129_22:40:53][28549.634939] Backtrace for cpu 2 (current):
[20180129_22:40:53][28549.635653] [<c004a410>] (unwind_backtrace+0x0/0xf8) from [<c0049408>] (smp_send_all_cpu_backtrace+0x60/0xdc)
[20180129_22:40:53][28549.637085] [<c0049408>] (smp_send_all_cpu_backtrace+0x60/0xdc) from [<c00cda34>] (__rcu_pending+0x144/0x3c0)
[20180129_22:40:53][28549.638455] [<c00cda34>] (__rcu_pending+0x144/0x3c0) from [<c00ce5c0>] (rcu_check_callbacks+0x11c/0x204)
[20180129_22:40:53][28549.639861] [<c00ce5c0>] (rcu_check_callbacks+0x11c/0x204) from [<c008ef00>] (update_process_times+0x38/0x68)
[20180129_22:40:53][28549.641320] [<c008ef00>] (update_process_times+0x38/0x68) from [<c00ae5ec>] (tick_sched_timer+0x80/0xe4)
[20180129_22:40:53][28549.642726] [<c00ae5ec>] (tick_sched_timer+0x80/0xe4) from [<c00a2040>] (__run_hrtimer+0x80/0x2c0)
[20180129_22:40:53][28549.644049] [<c00a2040>] (__run_hrtimer+0x80/0x2c0) from [<c00a2f3c>] (hrtimer_interrupt+0x118/0x294)
[20180129_22:40:53][28549.645389] [<c00a2f3c>] (hrtimer_interrupt+0x118/0x294) from [<c003d334>] (do_IPI+0x14c/0x208)
[20180129_22:40:53][28549.646595] [<c003d334>] (do_IPI+0x14c/0x208) from [<c0042a4c>] (__irq_svc+0x4c/0xe8)
[20180129_22:40:53][28549.647762] Exception stack(0xd6075f90 to 0xd6075fd8)
[20180129_22:40:53][28549.648497] 5f80:                                     c08b6168 80030093 00000001 00000000
[20180129_22:40:53][28549.649622] 5fa0: d6074000 c07b1c64 c0771a70 c057e304 c077a04c 412fc09a 00000000 00000000
[20180129_22:40:53][28549.650840] 5fc0: 00000000 d6075fd8 c0052540 c0043b44 40030013 ffffffff
[20180129_22:40:53][28549.650859] [<c0042a4c>] (__irq_svc+0x4c/0xe8) from [<c0043b44>] (default_idle+0x24/0x28)
[20180129_22:40:53][28549.650874] [<c0043b44>] (default_idle+0x24/0x28) from [<c0043e6c>] (cpu_idle+0xe0/0x124)
[20180129_22:40:53][28549.650890] [<c0043e6c>] (cpu_idle+0xe0/0x124) from [<105708d4>] (0x105708d4)
[20180129_22:40:53][28549.650898]
[20180129_22:40:53][28549.650900] sending IPI to all other CPUs:
[20180129_22:40:53][28549.650911] IPI backtrace for cpu 0
[20180129_22:40:53][28549.650916]
[20180129_22:40:53][28549.650921] Pid: 0, comm:              swapper
[20180129_22:40:53][28549.650931] CPU: 0    Tainted: G        W    (3.0.35-00073-geed2830 #52)
[20180129_22:40:53][28549.650942] PC is at default_idle+0x24/0x28
[20180129_22:40:53][28549.650954] LR is at arch_idle+0xbc/0xf4
[20180129_22:40:53][28549.650961] pc : [<c0043b44>]    lr : [<c0052540>]    psr: 400f0013
[20180129_22:40:53][28549.650966] sp : c075dfb0  ip : 00000000  fp : 00000000
[20180129_22:40:53][28549.650972] r10: 00000000  r9 : 412fc09a  r8 : c077a04c
[20180129_22:40:53][28549.650978] r7 : c057e304  r6 : c0771a70  r5 : c07b1c64  r4 : c075c000
[20180129_22:40:53][28549.650985] r3 : 00000000  r2 : 00000001  r1 : 200f0093  r0 : c08b6168
[20180129_22:40:53][28549.650994] Flags: nZcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[20180129_22:40:53][28549.651002] Control: 10c53c7d  Table: 270a804a  DAC: 00000015

0 Kudos
Reply