Need to interface MT9P031 image sensor with imx6 dual scm, the output format of the camera is 12-bit Bayer RGB format, although the parallel camera port of the processor supports the Bayer RGB data, but it only supports 8-bit, 9-10 bit or 16 bit patterns.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need to interface MT9P031 image sensor with imx6 dual scm, the output format of the camera is 12-bit Bayer RGB format, although the parallel camera port of the processor supports the Bayer RGB data, but it only supports 8-bit, 9-10 bit or 16 bit patterns.

863 Views
ageete
Contributor II

Need to interface MT9P031 image sensor with imx6 dual scm, the output format of the camera is 12-bit Bayer RGB format, although the parallel camera port of the processor supports the Bayer RGB data, but it only supports 8-bit, 9-10 bit or 16 bit patterns. can we use 16 bit for 12 bit data with MSBs as 0

0 Kudos
1 Reply

480 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ashvin

official nxp bsps do not support such use case, may be useful to check

https://community.nxp.com/message/331888 

i.MX6 OV5647 Bayer sensor driver (ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0) 

imx6 bayer to yuv conversion 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos