IMX6Q Enet Cannot Reach 1000M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Enet Cannot Reach 1000M

Jump to solution
2,042 Views
javen
Contributor I

Can anyone help me? in my MX6Q custom board based on MX6QSD(imx_3.0.35_4.1.0), our 1GB RGMII ethernet can only work at speed 495Mbits/sec,

is this normal ? Which configuration will affect the speed?

=============================================

iperf -c 192.168.122.125 -u -b 800M -t 10 -l 1000

------------------------------------------------------------

Client connecting to 192.168.122.125, UDP port 5001

Sending 1000 byte datagrams

UDP buffer size:  208 KByte (default)

------------------------------------------------------------

[  3] local 192.168.122.6 port 45130 connected with 192.168.122.125 port 5001

[ ID] Interval       Transfer     Bandwidth

[  3]  0.0-10.0 sec   590 MBytes   495 Mbits/sec

[  3] Sent 618437 datagrams

[  3] WARNING: did not receive ack of last datagram after 10 tries.

Labels (2)
Tags (3)
1 Solution
1,837 Views
gary_bisson
Senior Contributor III

Hi Javen,

This is a known issue. Please read the "Chip Errata for the i.MX 6" and look for the ERR004512:

  • The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps.
  • Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to 1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher than 400 Mbps, there is a risk of ENET RX FIFO overrun.
  • There is no workaround for the throughput limitation.

Regards,

Gary

View solution in original post

1 Reply
1,838 Views
gary_bisson
Senior Contributor III

Hi Javen,

This is a known issue. Please read the "Chip Errata for the i.MX 6" and look for the ERR004512:

  • The theoretical maximum performance of 1 Gbps ENET is limited to 470 Mbps.
  • Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to 1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher than 400 Mbps, there is a risk of ENET RX FIFO overrun.
  • There is no workaround for the throughput limitation.

Regards,

Gary