About IMX6Solo IBIS model.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About IMX6Solo IBIS model.

ソリューションへジャンプ
1,754件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has below question.Would you please advice.

Customer will use the EIM terminal to communication of data and the address of the FLASH ROM.

IBIS model such as described on

[Model Selector] gpio in IBIS model

gpio3p3_ds100_sr100_mio GPIO, 3.3V, extra drive, fast sr, slow fsel.

Please advice me , Whether the numerical value of this ds and sr that corresponds to  the value of the register set of Application Manual or Data sheets?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,675件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

please look at descriptions in

sect.9.5.2 [Model Selector] gpio i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

sect.36.4.258 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_RW)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,676件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

please look at descriptions in

sect.9.5.2 [Model Selector] gpio i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

sect.36.4.258 Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_EIM_RW)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信