IMX6D LDO2P5/VDD_HIGH_CAP Voltage Tolerance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D LDO2P5/VDD_HIGH_CAP Voltage Tolerance

Jump to solution
1,849 Views
tomsaluzzo
Contributor III

On the IMX6D, what is the tolerance on the VDD_HIGH_CAP output voltage from LDO2P5? For example, assume that the
VDD_HIGH_CAP output voltage is programmed to be 2.5V. What voltage range should
I expect to see on the VDD_HIGH_CAP output?

Labels (2)
1 Solution
1,664 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

The on-chip LDOs provide a precise, low voltage ripple power supply. The VDD_HIGH_CAP corresponds to the LDO_2P5. Accuracy should be around +-5% due to the nature of the analog LDO although there is no definitive number on the documentation that I’m aware of.

View solution in original post

1 Reply
1,665 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

The on-chip LDOs provide a precise, low voltage ripple power supply. The VDD_HIGH_CAP corresponds to the LDO_2P5. Accuracy should be around +-5% due to the nature of the analog LDO although there is no definitive number on the documentation that I’m aware of.