IMX6D LDO2P5/VDD_HIGH_CAP Voltage Tolerance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6D LDO2P5/VDD_HIGH_CAP Voltage Tolerance

ソリューションへジャンプ
1,842件の閲覧回数
tomsaluzzo
Contributor III

On the IMX6D, what is the tolerance on the VDD_HIGH_CAP output voltage from LDO2P5? For example, assume that the
VDD_HIGH_CAP output voltage is programmed to be 2.5V. What voltage range should
I expect to see on the VDD_HIGH_CAP output?

ラベル(2)
1 解決策
1,657件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

The on-chip LDOs provide a precise, low voltage ripple power supply. The VDD_HIGH_CAP corresponds to the LDO_2P5. Accuracy should be around +-5% due to the nature of the analog LDO although there is no definitive number on the documentation that I’m aware of.

元の投稿で解決策を見る

1 返信
1,658件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,

The on-chip LDOs provide a precise, low voltage ripple power supply. The VDD_HIGH_CAP corresponds to the LDO_2P5. Accuracy should be around +-5% due to the nature of the analog LDO although there is no definitive number on the documentation that I’m aware of.