IMX6 with 32bit DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 with 32bit DDR3

1,621 Views
omrisarfati
Contributor III

hello,

I'm designing a PCB with IMX6Q connect to 512MByte DDR3 (2 chips) with a 32 bit data bus. how i should connect the unused pins (DRAM_D32:63, DRAM_SDQS4:7,DRAM_SDQS_B4:7  and DRAM_DQM4:7)? leave floated , ground... ?

thanks,

omri

Labels (1)
0 Kudos
Reply
2 Replies

1,358 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi,

If you try searching the community for 32 bit ddr3 you would find numerous hits that would help you here -

Appropriate termination for unused DDR3 pins on a i.MX6 dual/quad design with 32-bit bus 

https://community.nxp.com/message/589115 

I.MX6 Dual with 32 bit DDR3

There are other threads also that may be of use/interest.

Regards

Ross

1,358 Views
omrisarfati
Contributor III

Thanks

0 Kudos
Reply