I.MX6 Dual with 32 bit DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 Dual with 32 bit DDR3

3,191 Views
cocobat
Contributor I

Hi all,

Here i have a question about the DDR3 connection.

we plan to use I.MX6 Dual in application, it has 64bit DDR3 interface, but we only want to use 32bit DDR3, cause we are afraid the PCB space is to tight for 4 DDR3.

in this condition, is it possible that just connect 2 DDR3 on MMDC, and leave other DDR signal floating?

and is it easy to do the modification in Linux source code for 32bit DDR3 interface?

thanks in advance.

LEON

Labels (2)
0 Kudos
Reply
3 Replies

2,585 Views
cocobat
Contributor I

Hi Igor,

It's great, thanks for your reply.

LEON

0 Kudos
Reply

2,585 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lei

yes this is possible, porting recommendations one can find in

i.MX_6Dual6Quad_BSP_Porting_Guide.pdf

L3.0.35_4.1.0_LINUX_DOCS

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,585 Views
vivekr
Contributor I

Hi

I am using Dual lite processor and due to PCB space constraints I am also about to use 32bit DDR interface instead of 64bit.

Is it ok leave to leave the unused pins(DRAM_SDCLK,DRAM_D, DRAM_DQM, DRAM_SDQS and nDRAM_SDQS)  floating?

Thank you,

Vivek

0 Kudos
Reply