IMX6-LAN7500 interface not able to fetch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6-LAN7500 interface not able to fetch

1,591 次查看
srikanthmediset
Contributor I

Hi,

    I was working on an customised iMX6 board with two ethernet hubs.One ethernet is detecting as eth0 and was working fine.The second was an POE ethernet of chipset LAN7500.When I try to config this ethernet it was throwing an error like

ifconfig eth1

eth1: error fetching interface information: Device not found

 When I go to the following path cd /etc/udev/rules.d/70-persistent-net.rules I was able to see the eth1 name for that interface.

 Now,I am not able to understand what is the conflict here I was facing.

Regards,

srikanth.

标签 (2)
0 项奖励
回复
2 回复数

1,444 次查看
b36401
NXP Employee
NXP Employee

It seems there is no driver for LAN7500 in your system. Please grep dmesg for "eth1".
You need to add the driver to the kernel.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,444 次查看
srikanthmediset
Contributor I

Hi victor,

    LAN7500 driver was inbuilt in the kernel. When I boot the board I was getting the log as below

    usbcore: registered new interface driver smsc75xx
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

      The above lines doesn't mean that the driver is ready to work????

    After entering into root when I run lsusb I was getting like

    Bus 002 Device 002: ID 0424:2514 Standard Microsystems Corp. USB 2.0 Hub

  

  where 0424 is the vendor id for smsc7500.

Regards,

srikanth.

0 项奖励
回复