Boundary Scan of I.MX515

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Boundary Scan of I.MX515

1,285件の閲覧回数
youngchan
Contributor I

Can't enter into boundary scan mode when debug MCIMX515DJM8C.Only can read high with INSTRUCTION_CAPTURE.

I test it with MX51_19x19_TO3_BSDL_1.BSDL,which is dowloaded in NXP official website.

If it need some other sequence to enter into the boundary scan mode?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,124件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Young

for boundary scan  JTAG_MOD (SJC_MOD)
should be high level,  this pin is sampled at TRST reset.
Other jtag signals are described in Table 4 "JTAG Controller
Interface Summary" i.MX51 Datasheet. Please check that these signals are
voltage level comparible with used jtag hardware.
http://www.nxp.com/docs/en/data-sheet/IMX51AEC.pdf
 Also please check that clocks are present on i.MX51 - crystal 24MHz and CKIL.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,124件の閲覧回数
youngchan
Contributor I

Thanks verify much.It is ok now.

0 件の賞賛
返信