IMX6 Android oreo booting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Android oreo booting

4,357 Views
vinays
Contributor II

Hi,

I am using the MCIMX6DP7CVT8AA  processor in one of my projects and the android version is  Android O8.0.0_1.0.0 (Linux 4.9 kernel). I was trying to port the android 8 into my board but the android bootup is not getting completed, it is being stopped after starting the boot animation service.

Till here I am able to see the android logo on my display after this the launcher screen is not being invoked. Help me out with this issue.

Note: Please find the log attached.

Regards,

Parvathi

0 Kudos
Reply
5 Replies

4,332 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which display for your board? Have you finished the porting and set right kernel command in u-boot?

0 Kudos
Reply

4,328 Views
vinays
Contributor II

Yes I have finished the kernel porting and the uboot command I used is:

console ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,fbpix=RGB666,bpp=32 video=mxcfb1:dev=ldb,fbpix=RGB666,bpp=32 video=mxcfb2:off video=mxcfb3:off vmalloc=128M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=448M galcore.contiguousSize=33554432 buildvariant=userdebug androidboot.serialno=100879d4e3167aba androidboot.soc_type=imx6qp androidboot.storage_type=sd gpt androidboot.serialno=100879d4e3167aba androidboot.soc_type=imx6qp androidboot.storage_type=sd gpt

and the display I am using is TX18D204VM0BVA.

0 Kudos
Reply

4,337 Views
vinays
Contributor II

Hi,

I am able to start the zygote services by running the commands in the script fsl_partition_script.sh manually, but these services are running in the starting-dying loop without further initiation of other services. What will be the cause for this issue?

Please suggest to me a method to come out this issue. 

Note: Please find the attached log

Regards,

Parvathi.

0 Kudos
Reply

4,325 Views
vinays
Contributor II

My booting is being looped after the register of Zygote socket it is not moving to further preload class and resources and service manager.

 

0 Kudos
Reply