IMX6 Android bsp can support MPEG2 interlaced stream decode ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 Android bsp can support MPEG2 interlaced stream decode ?

跳至解决方案
1,977 次查看
weikeng-jimmy
Contributor III

Hi Sir,

My customer want to decode MPEG2 video stream . When I link to website to playback and get "can't play" message.

But I used the VLC can decode the stream. All MPEG2 video in broadcast are interlaced.

http://srv2.mediagate.tv/mg/advantech/ch-sport5.ts.

So I.mx6 Android BSP can support HW deinterlacer ?

platform: Android 4.2.2 & Android 4.4.2

标签 (3)
0 项奖励
回复
1 解答
1,744 次查看
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,744 次查看
art
NXP Employee
NXP Employee

Yes, the i.MX6 Android BSP supports the deinterlace feature in IPU hardware.

Best Regards,

Artur

0 项奖励
回复
1,745 次查看
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

0 项奖励
回复