IMX6 Android bsp can support MPEG2 interlaced stream decode ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Android bsp can support MPEG2 interlaced stream decode ?

ソリューションへジャンプ
1,974件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

My customer want to decode MPEG2 video stream . When I link to website to playback and get "can't play" message.

But I used the VLC can decode the stream. All MPEG2 video in broadcast are interlaced.

http://srv2.mediagate.tv/mg/advantech/ch-sport5.ts.

So I.mx6 Android BSP can support HW deinterlacer ?

platform: Android 4.2.2 & Android 4.4.2

ラベル(3)
0 件の賞賛
返信
1 解決策
1,741件の閲覧回数
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,741件の閲覧回数
art
NXP Employee
NXP Employee

Yes, the i.MX6 Android BSP supports the deinterlace feature in IPU hardware.

Best Regards,

Artur

0 件の賞賛
返信
1,742件の閲覧回数
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

0 件の賞賛
返信