IMX6 Android bsp can support MPEG2 interlaced stream decode ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Android bsp can support MPEG2 interlaced stream decode ?

Jump to solution
1,967 Views
weikeng-jimmy
Contributor III

Hi Sir,

My customer want to decode MPEG2 video stream . When I link to website to playback and get "can't play" message.

But I used the VLC can decode the stream. All MPEG2 video in broadcast are interlaced.

http://srv2.mediagate.tv/mg/advantech/ch-sport5.ts.

So I.mx6 Android BSP can support HW deinterlacer ?

platform: Android 4.2.2 & Android 4.4.2

Labels (3)
0 Kudos
Reply
1 Solution
1,734 Views
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

View solution in original post

0 Kudos
Reply
2 Replies
1,734 Views
art
NXP Employee
NXP Employee

Yes, the i.MX6 Android BSP supports the deinterlace feature in IPU hardware.

Best Regards,

Artur

0 Kudos
Reply
1,735 Views
saurabh206
Senior Contributor III

Hi

Android BSP support mpeg2 video stream support.

Please check what is audio decoder in your .ts stream.

It may possible required audio decoder or parser support is not available.

This can be one of the possible reason for "can't play" message.

Thanks

Saurabh

0 Kudos
Reply