IMX535 and DDR3, needs pull ups?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX535 and DDR3, needs pull ups?

ソリューションへジャンプ
3,167件の閲覧回数
sherry_zahid
Contributor III

Hi,

Just wondering if I need any external pull ups on the data and address lines when interfacing the IMX535 with DDR3 modules (Micron MT41K512M16). Also, on page 153 of the Datasheet for the IMX535 it shows a table with "out of reset conditions" for all the IO pins (for the address and data bus for DDR3). For example it states for the pin "DRAM_A0" a config value of "LOW", does this mean no internal pull up is enabled or present on this line during reset? Thank you for your time and help.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,858件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

external pull ups are not needed, for connections example

one can look at

MCIMX53-START i.MX53 QS Board Schematics (REV 3)

i.MX53 Quick Start Board|Freescale

For "DRAM_A0" page 153 of the Datasheet meaning is that pull up is disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,859件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

external pull ups are not needed, for connections example

one can look at

MCIMX53-START i.MX53 QS Board Schematics (REV 3)

i.MX53 Quick Start Board|Freescale

For "DRAM_A0" page 153 of the Datasheet meaning is that pull up is disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,857件の閲覧回数
sherry_zahid
Contributor III

Hi Igor

Thanks for your reply. I also meant to ask, would there be any design violations if I tie all of the following ground pins together and route them to ground without any external pull resistor?

A1, A11, A13, A18, A2, A22, A23, AA11, AA15, AA20, AA21, AB1, AB18, AB2, AB22, AB23,

AC1, AC18, AC2, AC22, AC23, B1, B11, B13, B18, B23, C12, C20, C21, D19, E19, F19, F20,

F21, F22, G19, G7, H10, H12, H8, J11, J13, J15, J17, J20, J9, K10, K12, K14, K16, K21, K8,

L11, L13, L15, L7, L9, M10, M12, M14, M16, M8, N11, N13, N15, N9, P10, P12, P14, P16,

P21, P7, P8, R11, R13, R15, R17, R20, R9, T10, T14, T16, T8, U15, U19, V15, V18, V19,

V20, V21, V22, W19, Y14, Y15, Y19

Thanks again!

0 件の賞賛
返信
2,857件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sherry

no problem with such connection.

Best regards

igor

0 件の賞賛
返信
2,857件の閲覧回数
sherry_zahid
Contributor III

Thank you very much Igor, your prompt help and support is much appreciated.

Kind regards,

Sherry

0 件の賞賛
返信