IMX51 USB Host inicialization?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX51 USB Host inicialization?

ソリューションへジャンプ
1,619件の閲覧回数
wysockilukasz
Contributor II

Hello everybody,

I'm starting to work with imx51, and I have a problem with the initialization of the USB Host

working with IC-USB transceiver.

If any of you do something like that?

Thank you

Lukas

ラベル(1)
0 件の賞賛
返信
1 解決策
1,534件の閲覧回数
charleschang
Contributor III

Becaseu the usb phy interface follow the usb standard,

just use the official bsp kernel code, it initialized ok.

I've use 2 kinds of phy, both are ok.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,535件の閲覧回数
charleschang
Contributor III

Becaseu the usb phy interface follow the usb standard,

just use the official bsp kernel code, it initialized ok.

I've use 2 kinds of phy, both are ok.

0 件の賞賛
返信