IMX51 USB Host inicialization?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX51 USB Host inicialization?

Jump to solution
653 Views
wysockilukasz
Contributor II

Hello everybody,

I'm starting to work with imx51, and I have a problem with the initialization of the USB Host

working with IC-USB transceiver.

If any of you do something like that?

Thank you

Lukas

Labels (1)
0 Kudos
1 Solution
568 Views
charleschang
Contributor III

Becaseu the usb phy interface follow the usb standard,

just use the official bsp kernel code, it initialized ok.

I've use 2 kinds of phy, both are ok.

View solution in original post

0 Kudos
1 Reply
569 Views
charleschang
Contributor III

Becaseu the usb phy interface follow the usb standard,

just use the official bsp kernel code, it initialized ok.

I've use 2 kinds of phy, both are ok.

0 Kudos