IMX281 CAN Bus output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX281 CAN Bus output

Jump to solution
31,153 Views
annyli
Contributor II

The CAN_RX and CAN_TX can be connected to the CAN chip directly in my opinion. So why the EVK board use a buffer chip before CAN chip? Is it necessary?

Labels (1)
1 Solution
31,023 Views
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
31,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
31,023 Views
MartinHo
Contributor IV

The Buffers are used as level shifter (3.3V to 5V and 5V to 3.3V) if You use a 3.3V CAN-Bus Transceiver (for example SN65HVD232 from TI) they are not needed, or if You use a 5V type with TTL Inputs, You only have to reduce the RX output to 3.3V level .

Martin

31,023 Views
annyli
Contributor II

OK, I understand, thank you!:smileyhappy:

0 Kudos
Reply