IMX281 CAN Bus output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX281 CAN Bus output

跳至解决方案
29,670 次查看
annyli
Contributor II

The CAN_RX and CAN_TX can be connected to the CAN chip directly in my opinion. So why the EVK board use a buffer chip before CAN chip? Is it necessary?

标签 (1)
1 解答
29,540 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
29,541 次查看
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
29,540 次查看
MartinHo
Contributor IV

The Buffers are used as level shifter (3.3V to 5V and 5V to 3.3V) if You use a 3.3V CAN-Bus Transceiver (for example SN65HVD232 from TI) they are not needed, or if You use a 5V type with TTL Inputs, You only have to reduce the RX output to 3.3V level .

Martin

29,540 次查看
annyli
Contributor II

OK, I understand, thank you!:smileyhappy:

0 项奖励
回复