i.mx28 dynamic DDR size resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.mx28 dynamic DDR size resolution

942 次查看
matthevern
Contributor I

Hi All,

I was wondering if there was any mechanism to dynamically query or resolve the size of the DDR RAM chip which would be attached to the device.

I would like to be able to add a larger RAM chip without requiring a seperate firmware build specifically for the larger device.

Currently we are running with imx-bootlets.

Thanks.

Matt

标签 (1)
0 项奖励
回复
1 回复

814 次查看
igorpadykov
NXP Employee
NXP Employee

HI Matt

I am afraid this is not possible, also usually new DDR chip requires

rerunning ddr tests and tweaking pad drive strength.

Board Bring-up and DDR Initialization Tools

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复