IMX281 CAN Bus output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX281 CAN Bus output

ソリューションへジャンプ
31,125件の閲覧回数
annyli
Contributor II

The CAN_RX and CAN_TX can be connected to the CAN chip directly in my opinion. So why the EVK board use a buffer chip before CAN chip? Is it necessary?

ラベル(1)
1 解決策
30,995件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
30,996件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi anny

you are right: they can be connected directly.

EVK board was designed to provide as much possible connections

as possible to test all available interfaces and its options.

These buffers were added for flexibility,  for example MX28 EVK board supports

up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).

However, the 0 ohm options for CE2 and CE3 are disconnected by

default (they are used for CAN).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
30,995件の閲覧回数
MartinHo
Contributor IV

The Buffers are used as level shifter (3.3V to 5V and 5V to 3.3V) if You use a 3.3V CAN-Bus Transceiver (for example SN65HVD232 from TI) they are not needed, or if You use a 5V type with TTL Inputs, You only have to reduce the RX output to 3.3V level .

Martin

30,995件の閲覧回数
annyli
Contributor II

OK, I understand, thank you!:smileyhappy:

0 件の賞賛
返信