IMX 28 Linux /etc/network/interfaces missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 28 Linux /etc/network/interfaces missing

2,532 Views
ganeshh
Contributor III

Hi,

Am using IMX28 EVK along with Ltib Linux BSP 2.6.35. When i boot from the compiled images the /etc/network/interfaces is missing in root folder. Why is this happening? Is there any alternative file?

Tags (3)
0 Kudos
Reply
3 Replies

2,175 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Let me reproduce the problem.

Is there any modification you made?

Best Regards,

Alejandro

0 Kudos
Reply

2,175 Views
ganeshh
Contributor III

alejandrolozano

The freshly compiled Linux BSP image does'nt have Network folder and its components is /etc.

Its also lacking init.d folder which contains startup scripts and service command which is used to restart service...

What will be the problem??Should i change any setting in kernel config in order  to get these?

0 Kudos
Reply

2,175 Views
jamesbone
NXP TechSupport
NXP TechSupport

alejandrolozano, please give a comment on this?

0 Kudos
Reply