imx53qsb: STOP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx53qsb: STOP mode

1,972件の閲覧回数
warl0rd
Contributor I

Both  MCIMX53-START and MCIMX53-START-R board (aka imx53qsb, LOCO) boards run the Adeneo Android BSP 4.2. Is it possible to put those boards into the STOP mode as the Freescale Application note AN4270 mentions?? We are able to put the boards into the suspend mem mode and the total current consumption drops from 220 mA to 110mA (5V) which is still too much...

タグ(3)
0 件の賞賛
返信
4 返答(返信)

1,899件の閲覧回数
YixingKong
Senior Contributor IV

Warl0rd

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,899件の閲覧回数
warl0rd
Contributor I

The question is still unanswered, but this thread seems abandoned, you are free to close it right now.

0 件の賞賛
返信

1,899件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

AdeneoEmbedded do you have information or can you help with this question?

0 件の賞賛
返信

1,899件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信