IMX 28 Linux /etc/network/interfaces missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX 28 Linux /etc/network/interfaces missing

2,573 次查看
ganeshh
Contributor III

Hi,

Am using IMX28 EVK along with Ltib Linux BSP 2.6.35. When i boot from the compiled images the /etc/network/interfaces is missing in root folder. Why is this happening? Is there any alternative file?

标记 (3)
0 项奖励
回复
3 回复数

2,216 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Let me reproduce the problem.

Is there any modification you made?

Best Regards,

Alejandro

0 项奖励
回复

2,216 次查看
ganeshh
Contributor III

alejandrolozano

The freshly compiled Linux BSP image does'nt have Network folder and its components is /etc.

Its also lacking init.d folder which contains startup scripts and service command which is used to restart service...

What will be the problem??Should i change any setting in kernel config in order  to get these?

0 项奖励
回复

2,216 次查看
jamesbone
NXP TechSupport
NXP TechSupport

alejandrolozano, please give a comment on this?

0 项奖励
回复