I.MX8 Virtualisation Guide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX8 Virtualisation Guide

跳至解决方案
730 次查看
rishabh_modi
Contributor I

I was referring to the document IMXVIRTUG_ga  - i.MX Virtualization User's Guide

The document mentions the steps to boot and run Linux and Android simultaneously using Xen on I.MX Quad Max EVK board

 

1. Can the same steps and files be used to boot Linux and android on I.MX8 Quad Max MEK board?

2. Can the same steps be used to boot android automotive (14/15) with Linux using XEN?

0 项奖励
回复
1 解答
563 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

A: Yes, you can use this version and following the document but you need to run the Android P9.0.0_1.0.2-AUTO version BSP.

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

A:Just stop at the version mentioned in the document.

在原帖中查看解决方案

3 回复数
714 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

For your qustions:

1\No, for the guide just use for this version Linux Virtualization 4.14.98_4.11_0.10 GA (Based on Linux 4.14.98_2.0.0 BSP)

2\No, as you can see that in the released BSP that for the android 14/ andorid 15 do not support the XEN on the i.MX8QM, just support on the i.MX95.

Rita_Wang_0-1742542303052.png

And for the automotive adroid BSP do not support it.

 

0 项奖励
回复
701 次查看
rishabh_modi
Contributor I

rishabh_modi_0-1742546840856.png

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

0 项奖励
回复
564 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

A: Yes, you can use this version and following the document but you need to run the Android P9.0.0_1.0.2-AUTO version BSP.

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

A:Just stop at the version mentioned in the document.