I.MX8 Virtualisation Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8 Virtualisation Guide

Jump to solution
2,539 Views
rishabh_modi
Contributor I

I was referring to the document IMXVIRTUG_ga  - i.MX Virtualization User's Guide

The document mentions the steps to boot and run Linux and Android simultaneously using Xen on I.MX Quad Max EVK board

 

1. Can the same steps and files be used to boot Linux and android on I.MX8 Quad Max MEK board?

2. Can the same steps be used to boot android automotive (14/15) with Linux using XEN?

0 Kudos
Reply
1 Solution
2,372 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

A: Yes, you can use this version and following the document but you need to run the Android P9.0.0_1.0.2-AUTO version BSP.

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

A:Just stop at the version mentioned in the document.

View solution in original post

3 Replies
2,523 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For your qustions:

1\No, for the guide just use for this version Linux Virtualization 4.14.98_4.11_0.10 GA (Based on Linux 4.14.98_2.0.0 BSP)

2\No, as you can see that in the released BSP that for the android 14/ andorid 15 do not support the XEN on the i.MX8QM, just support on the i.MX95.

Rita_Wang_0-1742542303052.png

And for the automotive adroid BSP do not support it.

 

0 Kudos
Reply
2,510 Views
rishabh_modi
Contributor I

rishabh_modi_0-1742546840856.png

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

0 Kudos
Reply
2,373 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

This document also mentions only I.MX8 Quad Max EVK, but it has images for the MEK board also. 

1. Can I follow the same steps mentioned in the document to run android and linux on the I.MX Quad Max MEK ?

A: Yes, you can use this version and following the document but you need to run the Android P9.0.0_1.0.2-AUTO version BSP.

2. What is the latest android version for android automotive that will support xen with linux on I.MX Quad Max MEK?

A:Just stop at the version mentioned in the document.