I.MX6UL: Which USB-Interface is bootable ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6UL: Which USB-Interface is bootable ?

ソリューションへジャンプ
2,236件の閲覧回数
wowa
Contributor I

Hello Community,

i am looking after the USB-Interface. I want to boot and flash from the USB. I think this is the best way to debug this device.

Please can anyone tell me which USB-Port (1 or 2) has the highest priority for this task ?

Thanks and best regards.

ラベル(3)
0 件の賞賛
返信
1 解決策
2,110件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,110件の閲覧回数
wowa
Contributor I

Thx! That helps a lot !

BR

0 件の賞賛
返信
2,111件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信