I.MX6UL: Which USB-Interface is bootable ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL: Which USB-Interface is bootable ?

Jump to solution
2,260 Views
wowa
Contributor I

Hello Community,

i am looking after the USB-Interface. I want to boot and flash from the USB. I think this is the best way to debug this device.

Please can anyone tell me which USB-Port (1 or 2) has the highest priority for this task ?

Thanks and best regards.

Labels (3)
0 Kudos
Reply
1 Solution
2,134 Views
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,134 Views
wowa
Contributor I

Thx! That helps a lot !

BR

0 Kudos
Reply
2,135 Views
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply