I.MX6UL: Which USB-Interface is bootable ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX6UL: Which USB-Interface is bootable ?

跳至解决方案
2,275 次查看
wowa
Contributor I

Hello Community,

i am looking after the USB-Interface. I want to boot and flash from the USB. I think this is the best way to debug this device.

Please can anyone tell me which USB-Port (1 or 2) has the highest priority for this task ?

Thanks and best regards.

标签 (3)
0 项奖励
回复
1 解答
2,149 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,149 次查看
wowa
Contributor I

Thx! That helps a lot !

BR

0 项奖励
回复
2,150 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Walter

only USB OTG1 is used according to Figure 8-2. Serial Download Boot Flow

i.MX6UL Reference Manual http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复