I.MX6Q unit_test source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q unit_test source code

Jump to solution
2,199 Views
richarddestiny
Contributor III

Hi,all

       I buy the imx6q board from  the  third party,and  i can't see the  unit_test source code,also  i didn’t  get  from the  internet,

      can anybody offer me?

   thank you very much~

   wish you  have a  good day

Labels (1)
0 Kudos
Reply
1 Solution
1,942 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

please look at

Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0

Index of /buildsources/i/imx-test/imx-test-3.14.28-1.0.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,943 Views
igorpadykov
NXP Employee
NXP Employee

Hi Richard

please look at

Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0

Index of /buildsources/i/imx-test/imx-test-3.14.28-1.0.0

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,942 Views
richarddestiny
Contributor III

Hi,igor

       that is  what i’m looking for,thank you.

have a great day

richard

0 Kudos
Reply