How to use properly DDR3 calibration method of MPR and pre-defined value.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use properly DDR3 calibration method of MPR and pre-defined value.

ソリューションへジャンプ
1,517件の閲覧回数
takayuki_ishii
Contributor V

Hello, 

I have one question about proper use of DDR calibration method, with MPR and with pre-defined value.

In Read Calibration and Read DQS Gating Calibration, it have 2 metho, with MPR and with pre-defined value.

In what case are you supposed to use each function?

  with MPR : one time after board designed to generate pre-defined value.

  with pre-designed value : In product, one time in DDR initialization on power up sequence.

Is it correct?

Best regards,

Ishii.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,437件の閲覧回数
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The MPR method should be used once at the product bring-up stage to generate a pre-defined calibration value, that then should be used each time at power-on boot-up.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,438件の閲覧回数
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The MPR method should be used once at the product bring-up stage to generate a pre-defined calibration value, that then should be used each time at power-on boot-up.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,437件の閲覧回数
takayuki_ishii
Contributor V

Hello Artur

Thank you for your answer.

I will report it to my customer.

Best regards,

Ishii.

0 件の賞賛
返信