How to use properly DDR3 calibration method of MPR and pre-defined value.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use properly DDR3 calibration method of MPR and pre-defined value.

跳至解决方案
1,483 次查看
takayuki_ishii
Contributor V

Hello, 

I have one question about proper use of DDR calibration method, with MPR and with pre-defined value.

In Read Calibration and Read DQS Gating Calibration, it have 2 metho, with MPR and with pre-defined value.

In what case are you supposed to use each function?

  with MPR : one time after board designed to generate pre-defined value.

  with pre-designed value : In product, one time in DDR initialization on power up sequence.

Is it correct?

Best regards,

Ishii.

标签 (1)
0 项奖励
回复
1 解答
1,403 次查看
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The MPR method should be used once at the product bring-up stage to generate a pre-defined calibration value, that then should be used each time at power-on boot-up.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,404 次查看
art
NXP Employee
NXP Employee

Yes, your understanding is correct. The MPR method should be used once at the product bring-up stage to generate a pre-defined calibration value, that then should be used each time at power-on boot-up.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,403 次查看
takayuki_ishii
Contributor V

Hello Artur

Thank you for your answer.

I will report it to my customer.

Best regards,

Ishii.

0 项奖励
回复