How to update i.MX28 u-boot on NAND under u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to update i.MX28 u-boot on NAND under u-boot?

Jump to solution
1,264 Views
m_c
Senior Contributor I

We can update imx28_ivt_uboot.sb on NAND by kobs-ng with MfgTools. Can we boot from NAND with u-boot, then load imx28_ivt_uboot.sb via tftp and update it to NAND?

Labels (1)
0 Kudos
Reply
1 Solution
941 Views
igorpadykov
NXP Employee
NXP Employee

HI mc

I am afraid, not. However one can try to boot linux from

another media like sd and execute the same commands as

MFG Tools when updating nand.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
942 Views
igorpadykov
NXP Employee
NXP Employee

HI mc

I am afraid, not. However one can try to boot linux from

another media like sd and execute the same commands as

MFG Tools when updating nand.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply