How to update i.MX28 u-boot on NAND under u-boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update i.MX28 u-boot on NAND under u-boot?

ソリューションへジャンプ
1,282件の閲覧回数
m_c
Senior Contributor I

We can update imx28_ivt_uboot.sb on NAND by kobs-ng with MfgTools. Can we boot from NAND with u-boot, then load imx28_ivt_uboot.sb via tftp and update it to NAND?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
959件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI mc

I am afraid, not. However one can try to boot linux from

another media like sd and execute the same commands as

MFG Tools when updating nand.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
960件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI mc

I am afraid, not. However one can try to boot linux from

another media like sd and execute the same commands as

MFG Tools when updating nand.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信