mmc0: Timeout waiting for hardware interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc0: Timeout waiting for hardware interrupt

3,931件の閲覧回数
vineethhegde
Contributor II

Hai...

I am using i.MX6Q based board. Schematics is similar to the Sabre SD board. i got a error message as shown below.

>>> mmc0: Timeout waiting for hardware interrupt

Please suggest a solution.

ラベル(1)
0 件の賞賛
返信
1 返信

2,046件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vineeth113

seems sd port is not working correctly. Since you are using customizing BSP,

recommended to test board with Freescale BSP or with SDK. Also check signals

with oscilloscope, connecting to port sd card.

Best regards

igor

0 件の賞賛
返信