How to test USB2/3 eye pattern on iMX8m?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to test USB2/3 eye pattern on iMX8m?

2,362 Views
kevincheng
Contributor IV

Hi,

How to test USB2/3 eye patten on iMX8m on android os or linux os?  Thanks!!

Regards,

Kevin

0 Kudos
Reply
1 Reply

1,994 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,
The USB3 ports have a USB2 PHY and a USB3 PHY for backward compatibility. The USB2 PHY in this USB3 interface will use the same test procedures as for the USB2 port.
Below you could find reference material from the Community:
https://community.nxp.com/message/606950

https://community.nxp.com/docs/DOC-94460

USB3 (Superspeed) tests are totally different from USB2 and required different USB test equipment.
All USB test related information is available from the USB-IF web site at www.usb.org/compliance
At the bottom of the page there are links to pages with test specifications and procedures. Note also that i.MX USB testing is not specific. The test procedures are universal. Therefore, customers may be better served by contacting a USB test house for information. These test houses can perform the testing for the customer as USB3.x test equipment is quite specific and still very expensive.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply