i.MX6Q/eye pattern of USB HS1 setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q/eye pattern of USB HS1 setup

Jump to solution
6,605 Views
soichiyamamoto
Contributor V

Hi,

I develop a trial manufacture board of i. MX6 Quad and i. MX6 Dual-Lite.

I let you output a signal from the following pin and want to observe eye pattern to evaluate the signal quality on the board of USB I/F.

 ・i.MX6 Dual-Lite USB_H1_DP(E10)

 ・i.MX6 Dual-Lite USB_H1_DN(F10)

I refer to follows.

I.MX6 series USB Certification Guides​

Patch to make i.MX6DQ USB to support test modes for certification test

I set follows.

CCM_CCGR6_bit.CG1 = 3;
CCM_ANALOG_PLL_USB2_bit.POWER = 1;
USBC_UH1_USBCMD_bit.RST = 1;
USBC_UH1_USBMODE_bit.CM = 3;
USBC_UH1_PORTSC1_bit.PTC = 4;☆

A system is hung up when I set ”USBC_UH1_PORTSC1_bit.PTC”.

Is there the necessary setting anything else?

Best Regards,

soichi

Labels (2)
0 Kudos
Reply
1 Solution
4,421 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Have You tried FrankLiuapproach ?

---

Simple way to do the High Speed Host Electrical Test(including Eye Diagram) without PID/VID Test Fixture:

Use memtool to set the USB PHY registers Port Status & Control (USBC_n_PORTSC1)directly to output the specified pattern, make sure a HS device is connected to DUT before setting, otherwise system might crash.

memtool 0x2184184 1                           //read the register settings, address of the other USB port is 0x2184384

memtool 0x2184184=0x18441205      // Force to output Test Packet for Eye Diagram Test  

memtool 0x2184184=0x18411205      //Force to output J_STATE

memtool 0x2184184=0x18421205      // Force to output K_STATE

memtool 0x2184184=0x18431205      // Force to output SE0 (host) / NAK (device)

memtool 0x2184384=0x18001305      // Force to output Reset

memtool 0x2184384=0x18001285      //Ho Force to output Suspend

memtool 0x2184384=0x18001245      // Force to output Resume

---


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
4,422 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Have You tried FrankLiuapproach ?

---

Simple way to do the High Speed Host Electrical Test(including Eye Diagram) without PID/VID Test Fixture:

Use memtool to set the USB PHY registers Port Status & Control (USBC_n_PORTSC1)directly to output the specified pattern, make sure a HS device is connected to DUT before setting, otherwise system might crash.

memtool 0x2184184 1                           //read the register settings, address of the other USB port is 0x2184384

memtool 0x2184184=0x18441205      // Force to output Test Packet for Eye Diagram Test  

memtool 0x2184184=0x18411205      //Force to output J_STATE

memtool 0x2184184=0x18421205      // Force to output K_STATE

memtool 0x2184184=0x18431205      // Force to output SE0 (host) / NAK (device)

memtool 0x2184384=0x18001305      // Force to output Reset

memtool 0x2184384=0x18001285      //Ho Force to output Suspend

memtool 0x2184384=0x18001245      // Force to output Resume

---


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,421 Views
soichiyamamoto
Contributor V

Hi

Thank you.

What is DUT?

Which register is it?

Please give me a little more concrete information.

Best Regards,

soichi

0 Kudos
Reply
4,421 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.

DUT - Device Under Test

2.

To output signal for Eye Diagram Test (from i.MX6) :

$ memtool 0x2184184=0x18441205      // Force to output Test Packet

Regards,

Yuri.

0 Kudos
Reply