Hello,
I installed ubuntu image on iMX6 sabre lite board, I use LVDS panel now, I found the touch is not work. Could you give me suggestions how to make touch work?
I noticed that "ft5x06-ts 2-0038: ft5x06: Could not detect touch screen -19." during booting. Below is log from serial console.
Starting kernel ...
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
fsl-hdmi-dai hdmi_audio.3: failed to probe. Load HDMI-video first.
imx-audio-hdmi sound-hdmi.19: initialize HDMI-audio failed. load HDMI-video first!
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: Failed to bring link up!
imx6q-pcie 1ffc000.pcie: failed to initialize host
ft5x06-ts 2-0038: ft5x06: Could not detect touch screen -19.
ili210x_i2c 2-0041: i2c transfer failed
ili210x_i2c 2-0041: Failed to get firmware version, err: -5
egalax_ts 2-0004: Failed to read firmware version
tsc2004_reset: write_cmd -5
tsc2004 2-0048: Failed to reset TSC -5
ov5640_read_reg:write reg error:reg=300a
tc358743_read_reg:reg=0 ret=-5
tc358743_probe:cannot find camera
adv7180 2-0020: adv7180_read:read reg error: reg=11 ret=-5
tc358743_probe: failed, error=-19
mxc_v4l_open: Mxc Camera no sensor ipu1/csi0
mxc_v4l_open: Mxc Camera no sensor ipu0/csi0
mxc_v4l_open: Mxc Camera no sensor ipu0/csi0
mxc_v4l_open: Mxc Camera no sensor ipu1/csi1
update_device_addr: ov5642 ret=-5
ov5642_read_reg:write reg error:reg=300a
update_device_addr: ov5640_mipi ret=-5
ov5640_read_reg(mipi):reg=300a ret=-5
* Starting Bridge socket events into upstart[ OK ]
* Starting Bridge file events into upstart[ OK ]
[ OK ]
saned disabled; edit /etc/default/saned
Ubuntu 14.04.4 LTS nitrogen ttymxc1